Share
Linked In Facebook X (Twitter) Copy
Publication

Tool-Less Screws for VESA Mount

Share
Linked In
Facebook
Twitter
Copy
Share
banner image

Authors: 
Jui-Chieh Guo, Chenming Hsu, Fiona Hung, Ming-Lei Lin

Abstract:
This disclosure proposes a Tool-less method of attaching a Display to a VESA stand.

Background:
Currently, using a screwdriver/tool to set up the POS system is a common method.  We need to have the appropriate screw design to attach the display to different stand structures. You can spend much time and money on various attachment methods and screws.. This disclosure provides the solution to bring convenience to customers to install/remove the display on the VESA stand. The greatest benefit to the user is not needing any tool to tight the screws thereby saving time. They can easily assemble POS systems with this design and have a better user experience. The current design of the VESA stand is that the Display is attached to the stand by multiple screws.

This causes a few problems: It always requires a screwdriver to tighten /losen multiple screws when installing/removing the stand.  The screws are easy to lose when disassembling the stand.  

By using our design of tool-less screws, we could provide the following advantages.
Tool-less installation and removal of screws could Increase serviceability and shorten maintenance time. 

Description:
The user could take the display and face it down. Riveting the screw tight on the back of the iron plate. Take the mounting bracket and make sure all holes pass through the screw. Spin the wings on the screw and lock the display.

 

 

 

 

 

 

 

 

 

 

 

 

 

 

     

   Position for Insertion 

                           

 Rotate the Wings of the Screw Down        Slide Wings to Center to Secure Display

 

 

 

 

 

 

 

TGCS Reference 2468

Contact Intellectual Property department for more information