Share
Linked In Facebook X (Twitter) Copy
Patent

Methods and Systems Including an Edge Device Camera Configured to Capture Variable Image Data Amounts for Audited Shopping and Related Computer Program Products

Share
Linked In
Facebook
Twitter
Copy
Share

United States Patent
11,182,632

Title
Methods and Systems Including an Edge Device Camera Configured to Capture Variable Image Data Amounts for Audited Shopping and Related Computer Program Products

Abstract
A method of identifying an item as part of audited shopping can be provided by operating an edge device camera using a first operating parameter, detecting activity indicating a purchase of an item with view of the edge device camera, capture first image data for the item responsive to detecting the activity, processing the first image data to determine a shape of the item as viewed by the edge device camera, operating the edge device camera using a second operating parameter to capture second image data for the item that is greater than the first image data, responsive to determining that the shape of the item limits an accurate identification of the item using the first image data, processing the second image data to identify the item to provide an identified item, and operating the edge device camera using the first operating parameter.

 

 

Contact Intellectual Property department for more information