Share
Linked In Facebook X (Twitter) Copy
Patent

Methods and Systems Providing Synchronization of Data in a Distributed System Using Microservice Architecture in Servers, Store Controllers, Terminals and Related Articles of Manufacture

Share
Linked In
Facebook
Twitter
Copy
Share

United States Patent
11,645,302

Title
Methods and Systems Providing Synchronization of Data in a Distributed System Using Microservice Architecture in Servers, Store Controllers, Terminals and Related Articles of Manufacture

Abstract
A method of synchronizing data across an enterprise system including enterprise servers on an enterprise level and including store locations at a store level including edge devices operatively coupled to the enterprise servers can be provided by providing a changeplan that specifies updated data for microservice data operating within the enterprise system on an endpoint that utilizes the microservice in a microservice architecture to perform operations at a store location, executing the changeplan to initiate an export from an enterprise server that operates the microservice at the enterprise level to create an updated state for the microservice data on the endpoint, replicating the updated state for the microservice data at the enterprise server to provide an export updated state for the microservice data on the endpoint, storing the export updated state for the microservice data in an export table at the enterprise level, transmitting a message on a durable message bus from the enterprise level to the store level, initiating an import process at a store server responsive to receiving the message on the durable message bus and retrieving the export updated state for the microservice data from the export table.

 

 

Contact Intellectual Property department for more information