United States Patent
11,706,120
Title
Automated Process Flow Testing System
Abstract
Systems and methods of performing automated testing using a process flow of messages are provided. In one exemplary embodiment, a method includes receiving an indication that represents a time stamped message that is sent or received by a second electronic node and that is associated with a certain function. The method also includes generating a process flow of messages between the set of electronic nodes for the certain function based on the time stamped message of the second electronic node that is associated with the certain function and time stamped messages of the other electronic nodes associated with the same function so that the first electronic node is operable to simulate the certain function specific to that node based on the process flow of messages so as to test that at least one electronic node is operable to perform the certain function in conformance with the process flow of messages.