United States Patent
11,932,438
Title
Bag Rack
Abstract
A rotatable bag rack to support a plurality of bag types. The bag rack includes a stand and a rack. The rack is pivotally mounted to the stand so as to be rotatable about a pivot axis relative to the stand between a first position to hold a first bag type and a second position to hold a second bag type. The rack includes a pair of spaced apart arms to hold the first bag type that, in the first position, extends forward relative to the pivot axis. The rack, in the second position, extends downward relative to the pivot axis. The rack also includes a hanger fixed relative to the arms to hold a second bag type that, in the first position, extends backward relative to the pivot axis. The rack, in the second position, extends upward relative to the pivot axis.