Share
Linked In Facebook X (Twitter) Copy

United States Patent
11,985,778

Title
Bracket Assembly

Abstract
A bracket assembly with a latch plate and a lock plate. The lock plate is mounted in an overlapping arrangement with the latch plate and movable between an unlocked position and a locked position. First openings extend through the latch plate and are arranged to receive fasteners that protrude from the display. Second openings extend through the lock plate and are arranged to receive the fasteners. The second openings have a first portion aligning with the first openings in the latch plate when the lock plate is in the unlocked position to enable the bracket assembly to slide relative to the display in a first direction and a second portion enabling the lock plate to slide in a second direction relative to the latch plate between the locked and unlocked positions. A latch mechanism is configured to secure the lock plate in the locked position.

 

 

Contact Intellectual Property department for more information