United States Patent
12,126,619
Title
Point of Sale Controlling System
Abstract
Systems and methods of controlling a point of sale (POS) device are provided. In one exemplary embodiment, a method comprises, by a first network node that is operationally coupled to a POS device over a one-to-one connection, with the POS device being operable to receive commands related to secured and unsecured functions of the POS device that are sent to the first network node over the network and then conditionally sent by the first network node to the POS device over the one-to-one connection, receiving, from the second network node, an indication that includes both a command related to the POS device and a network node identifier associated with the second network node so that the first network node is enabled to authorize the second network node to send the command to the POS device based on the network node identifier and an authorized network node identifier.