The downloads below are restricted to those with an Enterprise ID (learn more)
Firmware for most devices can be upgraded automatically using either 4690 OS or UPOS drivers, or updated manually using the USB Diagnostics key package. However, some updates may have special requirements so please ensure you read the instructions that come with each update for more information.
Options and I/O Devices Service Guide
Common Packages
There are multiple cross-platform packages available (including Diagnostics, UPOS Drivers, RMA, MUS, NWD and VSP) as well as system unit drivers that apply to multiple machine types (including touch screen & biometric drivers)
View common packages & drivers
The document below shows which operating systems are supported across different processors and TGCS plaforms, to better enable viable operating system upgrade options for different POS terminal models.
TGCS hardware & OS compatibility matrix
If all you have is a 4-digit machine type or 7-digit machine-type/model number and you are not sure which product you have you can refer to the Support by Machine Type page.
Regulatory compliance documents can be found using the red Documentation & Publication icon at the bottom of the Support home page
This documents available include
- EU 617/2013 power consumption reports for system units
- Taiwan Bureau of Standards, Metrology and Inspection reports for Restriction of Hazardous Substance (RoHS)
- UN38.3 reports for shipping of lithium batteries
Machine type & model information
Most I/O devices are released as feature codes of the original system unit they are purchased with, but there are some devices that have their own machine type information.
Printers
Cameras
POS Peripheral Firmware, Publications & Utilities
|
POS Printers - 4610-1xx/2xx & 6145-1xx/2xx |


Common to 6145 and 4610 printers
List of approved thermal paper
6145-xTx / 4610-xxR Programming Guide
The printer font files includes the following languages:
TCx Printer 6145-2Tx (Dual Station) and 1Tx (Single Station)
Publications
6145-2Tx Installation & Service Guide
6145-1Tx Installation & Service Guide
Utilities
TCx Printer, unlike prior TGCS printer models, has a standalone program that can be used to directly configure the printer, and also to generate configuration files that the UPOS drivers can use to distribute the required configuration across the estate.
TCx Printer Configuration Utility User Guide (v10.01, 7 January 2026)
TCx Printer Configuration Utility for linux (v10.01, 7 January 2026)
TCx Printer Configuration Utility for Windows (v10.01, 7 January 2026)
Addition information for TCx Printer 6145-xTx Wired & Wireless models
WiFi firmware update and instructions (1.7.14)
SureMark 4610-2xR (Dual Station) and 1xR (Single Station)
Publications
4610-1xR Getting Started Guide
4610-2xR Getting Started Guide
Addition information for SureMark 4610-xxR Wired & Wireless models
4610-xxR Ethernet Adapter Guide
4610-xxR WiFi Adapter Installation and Management
4610-xxR WiFi Security Bulletin
Ethernet Configuration Utility Guide
Linux Configuration Utility (v1.0.67)
Windows Configuration Utility (v1.1.11)
SureMark 4610-Tx1/2/3/4/5/8/9 (Dual Station) and Tx6/7 (Single Station)
Support ended 1 Nov 2018. Refer to this web page (enterprise ID required) for more information, and for any available downloads and publications.
Firmware Files
| Description | Firmware Version | Firmware Files |
| 4610-xxR printer firmware | 1A.01 | Download |
| 6145-xTx printer firmware | 05.18.02 | Download |
|
POS Printers - 6180-S10 |

Important Notes
- The drivers to support these printers are different from all prior drivers for the 4610 and 6145 printers above.
- This means that the printer will not work with any existing TGCS drivers, including NWD, virtual serial port (VSP), OPOS & JavaPOS. For example, the 6180 printer will not show up in OposConfig or PosControlCenter. You must use the configuration program that comes with the relevant standalone drivers.
- The 6180 printer is NOT supported on 4690 or TCx Sky operating systems
- These printers do not use the same command set as prior 4610 or 6145 printers
- These printers do not follow the same firmware update process as prior 4610 or 6145 printers
Publications
Drivers
Printer Configuration Utility (v.6.0.3.0, 17 September 2025)
Windows virtual serial port driver (v.8.0.2.0, 17 September 2025)
Windows printer driver (v.13.0.3.0, 17 September 2025)
linux (CUPS) printer driver (v.6.0.2.0, 17 September 2025)
Android printer SDK (v.5.0.3.1, 17 September 2025)
iOS printer SDK (v.5.0.2.0, 17 September 2025)
Smart maintenance SDK (v.6.2.4.0, 17 September 2025)
Systems management drivers (v.3.0.1.0, 17 September 2025)
HTTP+JavaScript drivers (v.1.0.2.0, 17 September 2025)
|
HSP 100 / HSP-150 Receipt Printers |

Publications, drivers and firmware for HSP receipt printers and label printers can be found at
http://business.toshiba.com/support/
|
Cameras |
TCx Edgecam (6160-001 produce recognition camera)
Front End Produce Recognition Installation and Service Guide
Installation on the camera on a self-checkout lane is covered by the self-checkout publications
Software configuration of the camera is covered by the Elera publications.
TCx Edgecam+ (6260-001 loss prevention camera)
TCx EDGEcam+ Installation and Service Guide
|
POS Keyboards |

Modular POS Keyboards
Modular Keyboards Knowledgebase
Publications
Downloads
Modular Device Utility (v1.1.17, 3 October 2023)
The Modular Device Utility (MDU) also applies to the iButton reader and devices that contain certain models of MSR & keypads, such as 6149 TCx Display, TCx 800, and TCx 810/810e.
Modular Device CLI Utility (Command Line Interface) (v1.0.2.4, 13 August 2024)
The Modular Device CLI Utility (MDU CLI) also applies to the iButton reader and devices that contain certain models of MSR & keypads, such as 6149 TCx Display, TCx 800, and TCx 810/810e. This utility has a Command Line Interface that is operational for a local user
Firmware Files
For the latest keyboard firmware for USB devices refer to product IDs 460x & 467x in the list of USB firmware at the bottom of this page.
Firmware for the PS/2 modular keyboard is the same as its USB version. All other PS/2 keyboards are unsupported.
You cannot update firmware in RS485 keyboards. All RS485 keyboards are unsupported.
|
Standalone 2x20 / APA Displays |
All Models
Publications
Firmware Files
You cannot update firmware in RS232 & RS485 displays.
For the latest 2x20 firmware for USB displays refer to product ID 4524, 4525, 452A in the list of USB firmware at the bottom of this page.
For displays that are attached to the top of the system unit (IE, SurePOS 500, TCxWave, TCx 800) see the relevant section below.
|
SurePoint Display (4820) |

All Models
4820 SurePoint & 6149 TCxDisplay Knowledgebase
Firmware Files
4820-21x / 2Lx / 51x / 5Lx
Touch & video firmware is updated using Monitor Update Solution (MUS). Firmware files are shipped as part of the MUS package.
I/O device firmware (MSR, keyboard, etc) is found in the list at the bottom of the page
Other 4820 models
Support has ended for older models of 4820, refer to the End of Engineering Support announcements for more information.
|
TCx Display (6149) |

All Models
4820 SurePoint & 6149 TCxDisplay Knowledgebase
Downloads
For the Modular Device Utility (to configure wedge-mode MSR & keypad settings) use the link listed in the POS Keyboard section above.
Firmware Files
Firmware files can be found in different locations depending on function & display model.
6149-5xx models
Touch & video firmware is updated using Monitor Update Solution (MUS). Firmware files are shipped as part of the MUS package.
I/O device firmware (MSR, keyboard, etc) is found in the list at the bottom of the page
6149-Bxx / Wxx models
Touch firmware is updated using TCx Touch Updater or USB diagnostics key Touch firmware is shipped as part of the TCx Touch Updater package. It's also available here if you want to use the USB diagnostics key instead.
Video firmware is updated using Monitor Update Utility, USB diagnostics key or UPOS Firmware files are found at the bottom of this page.
I/O device firmware (MSR, keyboard, etc) is found in the list at the bottom of the page
|
TCx Touch Display (6150) |

All Models
4820 SurePoint & 6149 TCxDisplay Knowledgebase
Downloads
For the Modular Device Utility (to configure wedge-mode MSR & keypad settings) use the link listed in the POS Keyboard section above.
Firmware Files
Touch firmware is updated using TCx Touch Updater or USB diagnostics key
Firmware files are included in the firmware files package of the USB diagnostics key.
Video firmware is updated using USB diagnostics key or UPOS drivers Firmware files are found at the bottom of this page.
I/O device firmware (MSR, keyboard, etc) is found in the list at the bottom of the page
|
SurePOS 500 (4852) |

All Models
Firmware Files
The MSR firmware version depends on the age of the MSR (not the age of the SurePOS 500, since a FRU part could be newer than the original). There are currently 4 versions of firmware - A, B, C & D (also known as 1.x, 2.x, 3.x & 4.x).
Note that you cannot upgrade between versions (from A to B or B to C), you can only upgrade/downgrade within the same 'family' of firmware.
| Description | Version | Firmware File |
| SP500-xx1 & -xx2 | n/a | MSR can not be flashed with new firmware |
| SP500-xx3, -xx4 & -xx5 | A29 |
|
| SP500-x6x, x7x & x8x | B48 | |
| SP500-x6x, x7x & x8x | C48 | |
| SP500-x6x, x7x & x8x | D48 |
Windows MSR configuration utility
|
TCxWave (6140) I/O Head |

All Models
MSR Knowledgebase
2x20 Displays Knowledgebase
TCxWave Knowledgebase
Downloads
MSR command line utility v1.62b
MSR GUI utility v3.15
Head I/O firmware upgrade guide
Firmware Files
Firmware files can be found in different locations depending on function.
Touch & video firmware is updated using Monitor Update Solution (MUS). Firmware files are shipped as part of the MUS package.
I/O device firmware (MSR, keyboard, etc) is found in the list at the bottom of the page
Be aware that if you are upgrading firmware from an I/O head that currently has firmware < 0128 then you will also need to update the MSR configuration (even if you are a OPOS, JPOS or 4690 user). Open an SR to Support for instructions on how to do this.
|
TCx 800 (6200) |

All Models
MSR Knowledgebase
2x20 Displays Knowledgebase
TCx 800/810/810e Knowledgebase
Downloads
For the Modular Device Utility (to configure wedge-mode MSR & keypad settings) use the link listed in the POS Keyboard section above.
Firmware Files
Touch firmware is updated using TCx Touch Updater or USB diagnostics key
Firmware files are included in the firmware files package of the USB diagnostics key.
Video firmware is updated using UPOS or USB diagnostics key Firmware files are found at the bottom of this page.
I/O device firmware (MSR, keyboard, etc) for TGCS devices is found in the list at the bottom of the page.
|
TCx 810 (6201) & 810E (4828) |

All Models
MSR Knowledgebase
2x20 Displays Knowledgebase
TCx 800/810/810e Knowledgebase
Downloads
For the Modular Device Utility (to configure wedge-mode MSR & keypad settings) use the link listed in the POS Keyboard section above.
Firmware Files
Touch firmware is updated using TCx Touch Updater or USB diagnostics key
Firmware files are included in the firmware files package of the USB diagnostics key.
Video firmware is updated using UPOS or USB diagnostics key Firmware files are found at the bottom of this page.
I/O device firmware (MSR, keyboard, etc) for TGCS devices is found in the list at the bottom of the page.
|
TCx 820 (6225) |

All Models
MSR Knowledgebase
2x20 Displays Knowledgebase
TCx 800/810/810e Knowledgebase
Firmware Files
Touch firmware is updated using TCx Touch Updater or USB diagnostics key
Firmware files are included in the firmware files package of the USB diagnostics key.
Video firmware is updated using UPOS or USB diagnostics key Firmware files are found at the bottom of this page.
I/O device firmware (MSR, keyboard, etc) for TGCS devices is found in the list at the bottom of the page.
|
Scanners and Scales |
All Models
Scanners & Scales Knowledgebase
Firmware Files
TGCS does not provide firmware updates for scanners or scales, since we do not manufacture them. However, both UPOS and 4690 OS will update OEM scanners and scales with the update file provided by the device manufacturer. Contact the relevant OEM for the new firmware file, then follow the normal UPOS and 4690 OS procedures to apply the new firmware to your device.
|
Cash Drawers |
All Models
Publications
Firmware Files
For the latest firmware download refer to product IDs 4550-455A in the list of USB firmware at the bottom of this page.
|
Biometric Devices |
All Models
The fingerprint reader is an ordering option for modular POS keyboards and select models of TCxWave, TCx800, TCx810 & 810e, TCxDisplay and SurePOS 500.
Drivers and development kits for the biometric fingerprint reader are provided in this Knowledgebase article
Usage limitations are outlined in the relevant TGCS product Planning & Installation Guide
|
iButton |

All Models
For the latest firmware download refer to product ID 4502 in the list of USB firmware at the bottom of this page.
Be aware that updating to firmware 0122 will erase the USB serial # in the iButton head, due to a flaw in earlier firmware. This will not affect operation.
Downloads
For the Modular Device Utility (to configure wedge-mode settings) use the link listed in the POS Keyboard section above.
|
Firmware for TGCS USB POS Devices |
Firmware for USB devices is organised by ascending USB product ID.
Due to product age not all generations of firmware are supported any more (old versions are just posted here for reference), refer to the End of Engineering Support announcements for more information.
Due to chip shortages you may see multiple versions of firmware for the same device, this is normal and expected as we change the processor inside each device. You cannot upgrade a device from one generation to another.
Instructions for upgrading USB firmware are at the end of the table.
Notes
[1] 4610-Tx1/2 printers do not have a USB interface. These printers are no longer supported.
[2] 4610-Tx3/4/5/6/7 printers have separate firmware versions for the USB printer interface & printing functions. These printers are no longer supported.
[3] 4610-Tx8/9 printers have one consolidated firmware file for USB interface & printing functions. The firmware is updated via the printer interface, not the USB interface. These printers are no longer supported.
[4] 4610-xxR printers have one consolidated firmware file for USB interface & printing functions. The firmware is updated via the printer interface, not the USB interface. Printer firmware for these printers can be found at the top of the page in the POS Printer section.
[5] This is the same content as the MUS UP packages but suitable for use with UPOS & USB Diags.
Firmware Update Instructions
To update firmware using the USB Diagnostic Key....
1. Download the relevant firmware files listed above
2. Insert the TGCS USB diagnostics key into your PC
3. Copy the *.dat file(s) to \utilities\flash\usb_Firmware folder on the memory key
4. Eject the memory key from your PC. Install it into the POS system unit and reboot. You will need to manually update the firmware in the respective devices
To update firmware using OPOS driver on Windows
1. Download the relevant firmware files listed above
2. Copy the *.dat file(s) to the c:\pos\usb folder
3. Either reboot the POS system unit , use services.msc to restart the "Toshiba POS Startup Control" service, or use "net stop aipstartd" and "net start aipstartd" commands from an elevated command prompt.
To update firmware using JPOS driver on Windows
1. Download the relevant firmware files listed above
2. Copy the *.dat file(s) to the c:\pos\javapos\res\flash\usb folder
3. Either reboot the POS system unit , use services.msc to restart the "Toshiba JavaPOS Flash Utility" service, or use "net stop jposflashutility" and "net start jposflashutility" commands from an elevated command prompt.
To update firmware using JPOS driver on linux
1. Download the relevant firmware files listed above
2. Copy the *.dat file(s) to the /opt/tgcs/javapos/flash/usb folder
3. Restart the POS system unit
To update firmware using TCxSky
1. Download the relevant firmware files listed above
2. Follow the instructions in the OS community
|
Firmware for OEM USB POS Devices |
TGCS does re-sell OEM devices, and firmware for those devices is listed below.
Firmware for USB devices is organised by vendor and ascending USB product ID.
Firmware Update Instructions
Follow the instructions above for TGCS USB firmware update, host systems running TCx Sky or UPOS will update the scanner as if it's a TGCS device
Need help with your I/O Devices?
Submit a Service Request- ${title}${badge}