Machine type & model information
Machine type & model information for self-checkout lanes & self-service terminals.
Restricted content (security alerts, BIOS & publications)
6700-100 MxP Vision Kiosk
OS Drivers & Downloads
MxP Vision Kiosk only runs TCx Sky, so there are no separate OS downloads for it.
All OS configuration is via the relevant terminal load definition on the controller.
Publications
Hardware Planning & Installation Guide
6900-1xx Pro-X Hybrid Kiosk
OS Drivers & Downloads
Windows drivers for the POS terminal in the self checkout lane are listed by machine type on the relevant hardware page.
POS Devices - Printer & TAL (signal light)
There are no drivers built-in to any supported operating system (Windows, linux, or TCx Sky) that support this hardware out of the box, you will always need to download something additional no matter which operating system you use.
This is complicated product to configure, please make sure you have read the KB article, Pro-X Hybrid Kiosk driver architecture overview
OPOS (Windows) driver for printer & TAL (v4.0.6.0)
JavaPOS (Windows or linux) driver for printer & TAL (v2.22.6.0)
TCx Sky extension, containing JPOS drivers for printer & TAL & 4610 emulation firmware (v33)
UPOS systems management information (v1.2.0)
TAL (non-UPOS) API (Windows) (v1.1.2.0)
TAL (non-UPOS) API (linux) (v1.2.0.0)
TAL firmware (boot 0101 / main 0106)
Printer & TAL Configuration Utility (v2.4.0.0)
Printer (non-UPOS) driver (Windows) (v11.0.3.0)
VCOM (Windows) Driver (V7.0.1.0, 27 March 2025)
Printer firmware (boot 21.04 / main 51.54 / font 3.07 / table 51.05)
POS Devices - Scanner
Scanner drivers for WIndows & linux can be obtained directly from the relevant OEM, Datalogic or Zebra (depending on which hardware feature you ordered) or you can use the TGCS UPOS drivers if you prefer. Note that if you are running CHEC you must use the TGCS drivers, not the ones from the scanner vendor.
If you are using TCx Sky and downloaded the printer & TAL driver above then you also need the TGCS JPOS driver for the scanner (since all built-in OS support for all devices is disabled once you install any JPOS extension, and the built-in scanner driver that is included in the OS won't work any more).
TGCS drivers for all supported operating systems (Windows, linux & Tcx Sky) can be found on the common packages & drivers page.
Publications
KOP-3S01 Kiosk Printer User Manual
6800-K0x/K1x MxP Design Kit
OS Drivers & Downloads
Windows drivers for the POS terminal in the self checkout lane are listed by machine type on the relevant hardware page.
Publications
MxP Connection Guide (TCx 820)
Educational Service Video
Clearing combined coin recycler (CCR) coin jams
Note that a CCR is different from a bulk coin recycler (BCR)
6800-KDU Self Checkout Kit Of Parts
OS Drivers & Downloads
Windows drivers for the POS terminal in the self checkout lane are listed by machine type on the relevant hardware page.
Publications
Kit of Parts Connection Guide (TCx 810)
6800-4x0 Self Checkout
OS Drivers & Downloads
Windows drivers for the POS terminal in the self checkout lane are listed by machine type on the relevant hardware page.
POS Devices
There are no hardware drivers required for the cash devices or security scale, and access to those devices is controlled by the CHEC application.
Publications
Educational Service Video
Clearing combined coin recycler (CCR) coin jams
Note that a CCR is different from a bulk coin recycler (BCR)
6800-1x0 / 2x0 / 3x0 Self Checkout
OS Drivers & Downloads
Windows drivers for the POS terminal in the self checkout lane are listed by machine type on the relevant hardware page.
POS Devices
There are no hardware drivers required for the cash devices or security scale, and access to those devices is controlled by the CHEC application.
Publications
Chinees, Serbian, Russian, Ukrainian
Chinese, Serbian, Spanish, Russian, Ukrainian
4888-Exx / BW4 Self Checkout
OS Drivers & DownloadsWindows drivers for the POS terminal in the self checkout lane are listed by machine type on the relevant hardware page.
POS Devices
There are no hardware drivers required for the cash devices or security scale, and access to those devices is controlled by the CHEC application.
Publications
4888-Exx/BW4 Planning & Installation Guide
4888-Exx/BW4 Hardware Service Guide
4845-Xxx / BWx Self Checkout
Support ended 1 February 2020. Refer to this web page (enterprise ID required) for more information, and for any available downloads and publications.
4845-1xx / 6xx / 8xx / Wxx Self Checkout
Support ended 1 Nov 2018. Refer to this web page (enterprise ID required) for more information, and for any available downloads and publications.
4855-xxx Anyplace Checkout
Support ended 1 Nov 2018. Refer to this web page (enterprise ID required) for more information, and for any available downloads and publications.
Drivers & Information common to all products
There are multiple cross-platform packages available (including Diagnostics, UPOS Drivers, RMA, MUS, NWD and VSP) as well as system unit drivers that apply to multiple machine types (including touch screen & biometric drivers)
View common packages & drivers
The document below shows which operating systems are supported across different processors and TGCS plaforms, to better enable viable operating system upgrade options for different POS terminal models.
TGCS hardware & OS compatibility matrix
If all you have is a 4-digit machine type or 7-digit machine-type/model number and you are not sure which product you have you can refer to the Support by Machine Type page.
Security and vulnerability issues can be reported via the Product Security page
Regulatory compliance documents can be found using the red Documentation & Publication icon at the bottom of the Support home page. These documents available include
- EU 617/2013 power consumption reports for system units
- Taiwan Bureau of Standards, Metrology and Inspection reports for Restriction of Hazardous Substance (RoHS)
- UN38.3 reports for shipping of lithium batteries
- Turkish EPREL reports
Need help with your Self Checkout or Self-Service system?
Submit a Service Request- ${title}${badge}