Share
Linked In Facebook X (Twitter) Copy

Authors: 
Tim Crockett, Brad Johnson, Jack Ratcliffe

Abstract:
This solution provides a standardized mounting and Input/Output (IO) system that can allow multiple IO devices to be mounted to the outer edges of displays and All in One System units

Background:
For years we have been attaching Input/Output (IO) devices to the outside edge of our POS monitors, e.g., MSR readers, button readers, fingerprint readers, and cameras. Currently we create a custom port and mount point with a TTL or USB connector dedicated to the IO device. Then, later in the product life cycle we will decide that we want some other device connected to the edge of the monitor. This requires a new enclosure or adaptor to fit the new device to the old mount point. This solution provides a standardized mounting and IO system that can allow multiple IO devices to be mounted.

Description:
The solution proposes a standardized IO rail system that is built into the edges of the display with power and IO signals that allow multiple devices to attach. The IO system can be a single drop system such as USB or a multidrop system such as CAN bus with CAN bus being the most desirable since it would allow multiple devices with as few as 4 signals. For USB two extra signals would be required for each possible additional device.

See attached figures for details.

 

Claims:
Rail IO system for attaching input/output devices to the edges of a user interface screen such as MSR, fingerprint reader, etc

 

Supporting Art:

  • Wire harness
  • US CN JP CN108233283B 杉野秀寿 住友电装株式会社
  • Quick connect electrical box
  • US US7572976B1 Victor Merrill Victor Merrill
  • Display holder
  • CN CN104421594B 志煌 恩倍吉科技顾问(深圳)有限公司
  • Slide Rail Type Electrical Connecting System
  • KR KR102156890B1 양경호 양경호

 

TGCS Reference 4475

Contact Intellectual Property department for more information