Share
Linked In Facebook X (Twitter) Copy
Publication

Indicator Feature on SCO Camera

Share
Linked In
Facebook
Twitter
Copy
Share
banner image

Authors: 
Wayne Liu, Rebecca Hsiao, Kenter Su, Merrick Wang

Abstract:
The proposed solution provides a replacement for the current status light on a SCO(Self Check Out System).

Background:
In the current SCO structure, there are several kind of cameras assembled on the display or on the TAL(Transaction Awareness Light). And there are an indicator lights on the TAL. Our idea is to have the indicator feature on the cameras to replace the TAL indicator lights.

Description:
There are different cameras assembled on SCO. Our idea is to have translucent enclosure of the camera. A LED inside the camera housing. This camera can be the indicator of the SCO.
For example, this indicator would replace the current status light.
Red => SCO system abnormal or occupied
Green => normal or available
The indicator gives a concise status of the SCO.

 

TGCS Reference 3685

Contact Intellectual Property department for more information