Authors:
Jack Ratcliffe, Hye Suk Makley, Brian Rossi, Jared Schott
Abstract:
This disclosure proposes a system where 4 locking mechanisms turn simultaneously to secure the bagger cover to the bagging unit by limiting upward movement
Background:
The scales in bagging units require specific cover designs as to not disrupt the weight readings from the items that are placed in the bagging area. This means the covers cannot be rigid in the up/down direction. There is also a desire to prevent the covers from bouncing due to impact from dropped items or from being removed by unauthorized personnel. This system achieves these goals by fastening the cover to the scales using a series of locks while allowing a minimal upward motion while in the lock position. This ensures that the locks will not affect scale readings during normal operations while limiting the cover's movement to keep it within the designed area of operation.
Description:
See attached images for multiple locking methods for platen covers on bagging stations.
Usages:
Multiple methods to lock platen covers on bagging stations in place for security as well as safety from end user usage.
Enabling Technology:
Basic latching methods currently used by many industries.
Claims:
Method to lock platen covers on bagging stations in place for security as well as safety from end users, to prevent injuries.
TGCS Reference 1994