United States Patent
10,380,816
Title
Accessing a Secure Region of an Environment Using Visually Identified Behaviors Relative to an Access Control Device
Abstract
A method, computer program product, and system are disclosed for facilitating access by a first person to a secure region that is at least partly defined by an access control device. The method acquires, using at least one visual sensor, first image information including the first person and the access control device. The method identifies the first person using image analysis performed on the first image information. The method further identifies a first behavior of the first person relative to the access control device. Upon determining the first behavior corresponds to a predefined visual access behavior indicating that the first person is in the process of manually operating the access control device, and that the security level of the first person satisfies a predetermined threshold security level associated with the access control device, the method permits the first person to physically access the secure region.