United States Patent
9,164,740
Title
System and Method for Replacing Java Beans
Abstract
A method and apparatus is provided for reconfiguring application comprising a plurality of base code components at startup. A control application first retrieves the plurality of base components responsive to receiving a command to execute the application program. Prior to beginning execution, however, the control application replaces a selected base code component with another code component, and then subsequently replaces that newly inserted code component with yet another code component. Whether any given code component is to be replaced at startup is determined based on an annotation included in the code components. Once the application program has been reconfigured to include the appropriate code components, the application program is executed.