United States Patent
9,429,993
Title
Computing Device Docking Systems
Abstract
Computing device docking systems are disclosed. According to an aspect, a computing device docking system includes a docking station component having an opening defined within a surface. The system includes a pin including a body and an end having a member extending laterally from the body. The end of the pin is receivable within an opening of a computing device component for attaching the computing device component to the docking station. The pin is moveable within the opening between a first position and a second position. In the first position, at least a portion of the body and at least a portion of the member is positioned within the opening of the docking station component. In the second position, at least a portion of the body is within the opening and the member is outside of the opening of the docking station component.