Share
Linked In Facebook X (Twitter) Copy
Patent

Secure Self-Checkout

Share
Linked In
Facebook
Twitter
Copy
Share

United States Patent
8,746,557

Title
Secure Self-Checkout

Abstract
Under the present invention, item verification is automated and expedited. Specifically, items to be purchased can be scanned by the shopper using a barcode reader (e.g., a scanner) attached to or positioned near the shopping receptacle. As items are scanned, they are identified based on their barcode and added to an item list. Item verification can then performed at checkout using imaging technology. For example, the shopping cart or shopping basket can be brought into the field of view of a computer-connected camera. The camera and computer can, working from the customer's item list developed when the items are scanned, observe each product in the receptacle and "ring it up". If all products can be accounted for, the customer is free to leave; otherwise the customer is denied egress, informed of the problem, etc. A store employee can also be signaled to investigate. The total time required to make the decision is the time to take a picture and process it, which by human standards is very fast; faster than existing verification methods.

 

 

 

Contact Intellectual Property department for more information