Authors:
Hye Suk Makley, Kevin Gierl, Jack Ratcliffe
Abstract:
A mechanism is proposed that provides a lifting action for parts/assemblies that need service but there is no room for normal removal procedures. This particular design allows easy lift action of the scale pad to remove for service.
Background:
RVK design includes scale pad assembly, where it requires service from time to time. Currently it sits on top of the base frame where there is no room to carefully lift and remove for servicing.
This design allows easy lift action of the scale pad to remove for service.
Description:
The design considers the safety requirement of proper gap to eliminate pinch hazard.
The lever is pushed down to lift the scale pad to proper height needed to get one’s fingers underneath to lift up the assembly and remove it for service.
The level mechanism can also be designed such that it can be adjusted to the required height lift needed, depending on the size/weight/etc. of the item being lifted.
The rotating lever can also be designed such that it can be locked in place, so only managers can access to remove the item, for security related items.

Usages:
Applications can be used in any machines requiring service where part that need to be removed is encased and difficult to lift without aid, such as this design mechanism.
TGCS Reference 00203