All TGCS system units, and some I/O devices, are identified by a 4-digit machine type & 3-digit model number. Collectively this is known at machine type/model, or MTM.
The MTM & machine serial number can be found on a sticker on the front, side or bottom of each system unit. Note that serial numbers are not globally unique but they are unique across machine types.

Not all I/O devices & peripherals have machine types, some are just listed as feature codes of the original system unit.
Some items (mainly self-checkout & self-service) have 2 MTMs, one for the system unit and one for the self-checkout/self-service cabinetry and hardware.
Note that End of Service (EoS) and End of Engineering Support (EoES) are not the same thing; EoS is when we stop on-site service of the machine, EoES is when we stop doing updates (BIOS, firmware, etc) for it. The EoS and EoES dates are often not the same.
Some system units and I/O devices have already reach EoES status.
Any machine type not listed below is considered unsupported by product support & engineering teams.
System units & handhelds/tablets
| Machine Type |
Model |
Marketing Name |
Supported? |
Support page |
| 2001 |
100 |
TCx M1 |
Yes, but Advance Exchange only |
Handheld & Mobile Devices |
| 2011 |
100 |
TCx M11 |
Yes, but Advance Exchange only |
Handheld & Mobile Devices |
| 4750 |
All |
Toshiba Basics D10 |
No, has reached EoES status
(31 Dec 2023) |
EoES KB article |
| 4800 |
75x
7x1
7x2 |
SurePOS 700 |
No, has reached EoES status
(1 Nov 2018) |
EoES KB article |
7x3
7x4 |
SurePOS 700 |
No, has reached EoES status
(31 Dec 2019) |
| 4810 |
31x
32x
33x |
SurePOS 300 |
No, has reached EoES status
(1 Nov 2018) |
EoES KB article |
34x
35x |
SurePOS 300 |
No, has reached EoES status
(31 Dec 2023) |
36x,
37x,
38x |
TCx 300 |
Yes |
TCx 300 |
| 3x1 |
TCx 300 |
Yes |
TCx 300 |
| 4818 |
All |
Toshiba Basics T10 |
Yes |
Supported by the vendor directly |
| 4825 |
All |
TCx 620 |
Yes |
TCx 620 |
| 4828 |
All |
TCx 810 Essential |
Yes |
TCx 810E |
| 4836 |
All |
Anyplace Kiosk |
No, has reached EoES status
(1 Nov 2018) |
EoES KB article |
| 4838 |
3xx |
Anyplace Kiosk |
No, has reached EoES status
(13 Aug 2021) |
EoES KB article |
5xx
7xx
9xx |
Anyplace Kiosk |
No, has reached EoES status
(31 Jan 2021) |
| 4840 |
xx1
xx2
xx3
xx4 |
SurePOS 500 |
No, has reached EoES status
(1 Nov 2018) |
EoES KB article |
| 4845 |
1xx
6xx
8xx
Wxx |
Self Checkout |
No, has reached EoES status
(1 Nov 2018) |
EoES KB article |
Exx
Xxx |
Self Checkout |
No, has reached EoES status
(1 Feb 2020) |
| 4846 |
x5x |
SurePOS 500 |
No, has reached EoES status
(1 Nov 2018) |
EoES KB article |
| 4852 |
x2x |
SurePOS 500 |
No, has reached EoES status
(13 Aug 2021) |
EoES KB article |
| x6x |
SurePOS 500 |
No, has reached EoES status
(31 Jan 2021) |
x7x
x8x |
SurePOS 500 |
Yes |
SurePOS 500 |
| 4888 |
All |
Self Checkout |
Yes |
Self Checkout (System 6) |
| 4900 |
7x5 |
SurePOS 700 |
No, has reached EoES status
(31 Dec 2023) |
EoES KB article |
7x6
7x7 |
TCx 700 |
Yes |
TCx 700 |
| 4901 |
x1x |
TCx 900 |
Yes |
TCx 900 |
| 6140 |
1xx
x3x |
TCxWave |
No, has reached EoES status
(31 Dec 2024) |
EoES KB article |
x4x
x5x |
TCxWave |
Yes |
TCxWave |
| 6200 |
All |
TCx 800 |
Yes |
TCx 800 |
| 6201 |
All |
TCx 810 |
Yes |
TCx 810 |
| 6225 |
All |
TCx 820 |
Yes |
TCx 820 |
| 6700 |
All |
MxP Vision Kiosk |
Yes |
Self service |
| 6800 |
All |
Self Checkout |
Yes |
Self Checkout (System 7) |
| 6900 |
All |
Pro-X Hybrid Kiosk |
Yes |
Self service |
I/O Devices
For I/O devices that do not have an MTM you can find support on the I/O Devices support page.